This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: HET1 generates an wrong PWM frequency when the VCLK2 clock is not 75 MHz

Part Number: TMS570LC4357

Hi team,

Here's an issue from the customer may need your help:

HET1-16 generates the correct PWM frequency when VCLK2 is clocked at 75 MHz, while HET1-16 will generate incorrect PWM frequencies when VLCK2 is clocked at 50 MHz and 37.5 MHz.

Configure the VCLK2 clock to 37.5 MHz as shown in the figure below:

Enable N2HET1-16 to generate a frequency of 1KHz: 

Enable pins of N2HET1-16:

The PWM tested is as follows: 

Could you help look into this case? Thanks.

Best Regards,

Cherry