This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connection establishment from laptop to controller is not happeing (verified with ping)



Hi All,

I have used latest SDK(8.2.0.24) with kernel version 5.10.100  in this we are not able to ping from laptop to controller..

my architecture is laptop --> controller 

Task is to port from 4.9.59 kernel(sustom kernel) to 5.10.100

I am able to make the kernel up.. and we have used the KSZ8863 ethernet switch and can able to load the module.. while booting 

1 issue i am facing is i am not able to ping from laptop to controller(custom controller which is based on am335x.

Note: i have modified dts (am335x-evmsk.dts) i.e as below (5.10.100 kernel version)

&phy_gmii_sel {
rmii-clock-ext;
};

initialy it was because we wer using 4.9.59 kernel

&phy_sel {

 rmii-clock-ext;
};

will it be a problem while establishing connection? via ping?

am i missing any additional configurations..?

i debuged by wireshark and arp tool observed the arp is not able to reslove the ip.. may i know how resolve this..

Also 1 fundemnetal question: may i know who will be assigning ip for the controller?

please provide info at earliest..

Thank you