Part Number: LP-AM243
Other Parts Discussed in Thread: DP83869
Hi,
My customer is evaluating UDP operation using SDK sample (enet_cpsw_udpserver_am243x-lp_r5fss0-0_freertos_ti-arm-clang).
HW : LP-AM243 PROC109E3
SW : MCU PLUS SDK Version: 08.05.00.24
Q1) The example uses polling in RX task.
To improve performance, the customer wants to use an interrupt.
Is there an example using an interrupt?
Q2) Is 10Mbps operation supported?
The customer configure an external device as 10Mbps and LP-AM243 can link-up with it by auto-negotiation.
But it does not seem to communicate with 10Mbps.
Thanks and regards,
Koichiro Tashiro