Part Number: AM2634
Hello
For the Sitara AM263x we have 6 different Flash mode

What are differences for all Qspi boot mode? Could you explain them in more detail? I want to know, when is used individual boot modes ?
I have also got .cmm(am263x-S25FL128SA-qspi.cmm) file for the loading the software into the flash from you. Which mode should I use to load the code? Only DevBoot mode allows to load the code into the flash, but other modes do not allow me to load the code into the flash. Here in the .cmm file it is written I should choose Qsp_1. Which mode is Qsp_1 ?
I am a bit confused about this topic, maybe the topic is trivial but I need more information
Thanks in advance