This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: regarding eeprom acess of tms570ls3137 from hydac bsp 580

Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN

Hello good morning.,

Iam working an application, so I need to store some values in the EEPROM memory locations of TMS570LS3137 i.e., Bank-7(64KB),but Iam working on the HYDAC BSP 580 Which consists of TMS570LS3137,Can i use the library functions of HYDAAC BSP to access the eeprom of the tms570.since,the tms570 eeprom is not an external eeprom memory it is flash accumulated one .,The hydaac bsp library file of eeprom is shown below, Can i use it to access eeprom ?