Part Number: RM46L852
Hi,
I'm building a project using the TI ARM compiler (TI v20.2.7.LTS) configured for C11.
Because I'm not allowed to use dynamic memory allocation, I'm using C99 feature VLA.
The problem: by inspecting the internal of the VLA, I'm noticing that allocating a VLA calls __vla_alloc() that will use malloc to allocate memory.

I have looked in the ARM Optimizing C/C++ Compiler v20.2.0.LTS User's Guide without success.
I'm I correct that VLA actually does not use the stack?
Are VLAs guaranty to free the memory properly?
Are VLAs RTOS safe?
Is there a way to use those safely?
Is there an alloca function in the std library?
Regards,
Gabriel