Part Number: MSPM0G3505
Hello,
can the timer counter run with 80MHz? So max resolution is 12.5ps?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0G3505
Hello,
can the timer counter run with 80MHz? So max resolution is 12.5ps?
Regards, Holger
Hi Holger,
Yes, with one minor correction.
When sourcing from BUSCLK, any Power Domain 1 (PD1) Timer can operate at MCLK Frequency (up to 80MHz). This corresponds to 12.5ns though, not 12.5ps. TIMH0 in the MSPM0G3505 is in PD1.
Best Regards,
Brandon Fisher
Hi Brandon,
so TIMG (TIMG10), TIMA and TIMH can all run with 80MHz (on PD1) and have the same resolution.
Regards, Holger
Hi Holger,

Yes that is correct. Anything listed as PD1 should be able to run at 80Mhz.
Best Regards,
Brandon Fisher