Part Number: MCU-PLUS-SDK-AM263X
Hi,
Two issues to discuss:
1)
In section 4.17 (page 37) of the Hardware User's Guide (https://www.ti.com/lit/ug/spruj09c/spruj09c.pdf?ts=1676648505407: revised February 2023) I see that ADC2 inputs 2 through 5 are tied to GND through resistors. I also see that ADC4 inputs 2 and 3 are broken out to the HSEC connector.
This directly contradicts what I see in the PROC110E2 schematic.
On sheet 15 of the AM263x CC schematic (found in PROC110E2 design files folder at https://www.ti.com/lit/zip/sprcak1 : revised March 2022) I see that ADC2 inputs 2 and 3 are broken out to the HSEC connector. Only ADC2 inputs 4 and 5 are tied to GND through resistors. I also see that ADC4 inputs 2 and 3 are tied to GND through resistors, not broken out to the HSEC connector.
Which source (Hardware User Guide or PROC110E2 schematic) is correct?
2)
I see a possible error in the Hardware User Guide on page 38:
ADC2 mux selects ADC4 channels? Please confirm what is actually happening here.
Regards,
-Adrian