Part Number: RM48L952
Other Parts Discussed in Thread: UNIFLASH, HALCOGEN
Hi,
I have a problem with already programmed RM48L952 devices. We need to reprogram them using our own bootloader running from RAM(loaded in parallel mode using Boot ROM). If the device is blank, the bootloader works without any problems and everything is OK. But when we try to reprogram the devices(programmed with unknown data) our bootloader loaded to RAM not starts and also we are not able to debug this devices using Code Composer studio(we use the 12.2 ver). The OTP and AJSM is not prgrammed by this unknown code and only the flash is programmed.
The only way how we can access the devices is using the TI Uniflash. When we erase the device using this application, then we can access the devices and run the bootloader(and debug) without any problem. I can provide you the readed hex data of the flash from the devices(by UniFlash) but not in this public forum(if it is necessary). Also I can provide you the source code of our bootloader project(one zip file) for your investigation.
This is so time critical issue, so I will be appreciated for your help.
Tomas