Part Number: AM2432
Hello Support Team,
in our current project we want to use the AM2432 MCU with ECC memory. On the MCU_M4FSS we use the internal SRAM (256KB IMEM/DMEM with ECC). Now we want to test cyclically the ECC checker for diagnostic purpose. In chapter "12.6.4.3.6 Inject Only Mode" is written:
"There are modules that already perform the ECC generation and checking as part of their data path. In this case, the ECC wrapper may be configured in inject only mode, if needed. In this mode the ECC wrapper does not perform ECC detection and correction. The inject only mode allows users to inject single or double-bit errors so that the module logic can be tested for diagnostic purposes.
Note
There is no software control to enable inject only mode. It is configured via tie-off value. Inject only and ECC modes are mutually exclusive.
The interconnect ECC component also supports error injection mode. There is error injection logic for testing of the error checking logic (checkers)."
Does this mean, the diagnostic error injection is not working with the internal SRAM?
In a later project we want to use one R5F core with the 2MB SRAM (with ECC) and DDR4 (with inline ECC). Is the diagnostic error injection working on these ECC wrappers?
Best Regards,
Stephan