I was able to download the LM Flash Programmer utility. Is the utility used with the USB-micro port or the JTAG to perform the FW upgrade. After the image in the previous reply from Ti, reference is made to JTAG. If JTAG is used, are there jumpers that need to be set so U3 is updated and not U1?