Part Number: MSPM0G3507
Hi MSP Team,
Asking on behalf of a customer currently evaluating MSPM0G:
I have noticed that using the SDK and the linker-file that comes with it, mspm0g3507.lds (ti/devices/msp/m0p/linker_files/gcc/mspm0g3507.lds) does not configure size of the heap.
I can see at the top of that file that these are defined:
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x80; /* required amount of stack */
But they are not used anywhere in the actual the linker file. Thus the heap size end up being 0bytes.
I tried setting the heap (as described in this page) to 0x200 (using ". = . + _Min_Heap_Size;"):
But I am still not able to allocate memory from the heap. In one our MCU packages used for handling i2c properties the command realloc() is used and that seems to fail.
If I run the same code for allocating memory using ticlang instead, it works as expected, and memory is allocated. I can however not find the linker-file that ticlang is using.
Do you know what is causing this and do you have a working version of the linker file that actually uses _Min_Heap_Size and _Min_Stack_Size?
I have used mspm0_sdk_0_57_00_00_eng when I get this problem.
Please advice.
Thanks and regards,
/ Wolfgang