Part Number: TM4C129ENCPDT
Hi,
We have two external clocks connected one is XOSC 32kHz and another is OSC 25MHz. The CPU main clock is derived from OSC 25MHz and running a FreeRTOS based system. The Hibernate module is not required and hence not active nor I am using and RTC.
I have following questions;
- XOSC is 32kHz with Part number CMR200T-32.768KDZY-UT. Unfortunately this is not available anywhere. If you could suggest any alternative and reliable source.
- I am not sure if we even need this oscillator with the description I mentioned above. Please comment if the system will still work if this component is not installed ?
Thanks