Part Number: MSPM0G3505
Hi team,
MSPM0 G-Series MCUs Hardware Development Guide (slaae76a) states that "TI recommends connecting a combination of a 10-μF and a 0.1-nF low-ESR ceramic decoupling capacitor to the VDD and VSS pins Higher-value capacitors can be used but can impact supply rail ramp-up time." on page 2, below Note.

However, in Figure 1-1 and Figure 2-3, 10uF and 0.1uF are connected.

Which statement is correct?
Best regards,
Kurumi