Part Number: RM46L852
Other Parts Discussed in Thread: UNIFLASH
Hi. If this part is pre-programmed, can I reprogram without overwriting the original program settings?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Jagadish. No specifics. Just in general, if this device was initially programmed, can I reprogram?
Hi Ireen,
You can reprogram easily by the following two methods,
1. Using CCS (the project directly loaded into the device from CCS)
2. Using Uniflash (You can select the .out file of the project you want to reprogram and can load into the device).
You can refer below video to understand CCS method
LED blink program for Hercules controller - Google Search
--
Thanks & regards,
Jagadish.