Other Parts Discussed in Thread: TDA2
Hi TI Team,
Our HW platform is TI J6 ENTRY, SW is QNX660. We received a returned instrument from a customer with black screen. According to our analysis, the TI J6 ENTRY chip cannot work at -20 degrees.
Under normal temperature, the instrument works normally. When the chip surface temperature is cooled to -20 degrees Celsius, the chip cannot work. After normal temperature is restored, the chip can work normally and the operating system restarts.
The below test we have done:
1. DDR stress test, passed.
2.The data stored in emmc is normal which can run in other normal board.
3.Not found any coredump file in the target board, sw no error.
4.High temperature 80 degrees Celsius, passed.
5.Low temperature -40 degrees Celsius, not passed, using XDS200 debug, the PC pionter at 0x08049F84, the system not work.

6. VDD core voltage add 100mv,the issue still exists.
Questions:
Please help to analyse why l the J6 ENTRY chip can't not work under ow temperature?
Any questions or need more infos, please feel free to let me know.
BR,
Ryan