Part Number: EK-TM4C129EXL
Hi team,
My customer need assistance.
I am running my code and when I enter into my while loop, I pause it and get sent into the IntDefaultHandler function. I cannot find any issues with my code. I have the same functions used (with slight modifications) in a different project and it works just fine. I am attaching the 2 C files that I am having problems with, both are similar and the image from the Debugger.


#include <stdint.h>
#include <stdbool.h>
#define GPIO_PORTN ((volatile uint32_t *)0x40064000)
#define GPIO_PORTJ ((volatile uint32_t *)0x40060000)
#define GPIO_PORTK ((volatile uint32_t *)0x40061000)
#define GPIO_PORTF ((volatile uint32_t *)0x4005D000)
#define SYSCTL ((volatile uint32_t *)0x400FE000)
#define SysTick ((volatile uint32_t *)0xE000E000)
#define SYSCTL_MOSCCTL_PWRDN (1 << 3)
#define SYSCTL_MOSCCTL_NOXTAL (1 << 2)
#define SYSCTL_MOSCCTL_OSCRNG (1 << 4)
#define SYSCTL_RIS_MOSCPUPRIS (1 << 8)
#define SYSCTL_MISC_MOSCPUMIS (1 << 8)
#define SYSCTL_RSCLKCFG_OSCSRC_MOSC (3 << 20)
#define SYSCTL_RSCLKCFG_PLLSRC_MOSC (3 << 24)
#define SYSCTL_RSCLKCFG_NEWFREQ (1 << 30)
#define SYSCTL_RSCLKCFG_PSYSDIV_M (0x3ff >> 0)
#define SYSCTL_RSCLKCFG_PSYSDIV_3 3
#define SYSCTL_RSCLKCFG_USEPLL (1 << 28)
#define SYSCTL_RSCLKCFG_MEMTIMU (1 << 31)
#define SYSCTL_PLLFREQ0_MINT_S 0
#define SYSCTL_PLLFREQ0_MFRAC_S 10
#define SYSCTL_PLLFREQ0_PLLPWR (1 << 23)
#define SYSCTL_MEMTIM0_EBCHT_M (0b1111 << 22)
#define SYSCTL_MEMTIM0_EWS_M (0b1111 << 16)
#define SYSCTL_MEMTIM0_EBCE (1 << 21)
#define SYSCTL_MEMTIM0_FBCHT_3_5 (6 << 6)
#define SYSCTL_MEMTIM0_EWS_6 (6 << 16)
#define SYSCTL_MEMTIM0_FBCHT_M (0b1111 << 6)
#define SYSCTL_MEMTIM0_FWS_M (0b1111 >> 0)
#define SYSCTL_MEMTIM0_FBCE (1 << 5)
#define SYSCTL_MEMTIM0_FWS_6 (6 >> 0)
#define GPIO_PIN_0 (1 >> 0)
#define GPIO_PIN_1 (1 << 1)
#define GPIO_PIN_2 (1 << 2)
#define GPIO_PIN_3 (1 << 3)
#define GPIO_PIN_4 (1 << 4)
#define GPIO_PIN_5 (1 << 5)
#define GPIO_PIN_6 (1 << 6)
#define GPIO_PIN_7 (1 << 7)
#define LED1_PN1 GPIO_PIN_1
#define LED2_PN0 GPIO_PIN_0
#define LED3_PF4 GPIO_PIN_4
#define LED4_PF0 GPIO_PIN_0
#define SYSCTL_RCGCGPIO_PORTF (1 << 5)
#define SYSCTL_RCGCGPIO_PORTJ (1 << 8)
#define SYSCTL_RCGCGPIO_PORTK (1 << 9)
#define SYSCTL_RCGCGPIO_PORTN (1 << 12)
#define PUSH1_PJ0 GPIO_PIN_0
#define PUSH2_PJ1 GPIO_PIN_1
#define OUT_PK0 GPIO_PIN_0
#define OUT_PK1 GPIO_PIN_1
#define OUT_PK2 GPIO_PIN_2
#define OUT_PK3 GPIO_PIN_3
#define out (OUT_PK0 | OUT_PK1 | OUT_PK2 | OUT_PK3)
#define IN_PK4 GPIO_PIN_4
#define IN_PK5 GPIO_PIN_5
#define IN_PK6 GPIO_PIN_6
#define IN_PK7 GPIO_PIN_7
#define in (IN_PK4 | IN_PK5 | IN_PK6 | IN_PK7)
#define C 4778
#define D 4257
#define E 3792
#define G 3189
unsigned char index = 0;
const unsigned char sin[48] = {
0,0,1,1,1,2,2,3,4,5,6,7,8,9,10,11,12,13,13,14,14,14,15,15,
15,15,14,14,14,13,13,12,11,10,9,8,7,6,5,4,3,2,2,1,1,1,0,0
};
enum {
SYSCTL_RCGCGPIO = (0x608 >> 2),
GPIO_DEN = (0x51c >> 2),
GPIO_DIR = (0x400 >> 2),
GPIO_PUR = (0x510 >> 2),
SYSCTL_MOSCCTL = (0x07C >> 2),
SYSCTL_RIS = (0x050 >> 2),
SYSCTL_MISC = (0x058 >> 2),
SYSCTL_RSCLKCFG = (0x0B0 >> 2),
SYSCTL_PLLFREQ0 = (0x160 >> 2),
SYSCTL_PLLFREQ1 = (0x164 >> 2),
SYSCTL_MEMTIM0 = (0x0C0 >> 2),
SYSCTL_PLLSTAT = (0x168 >> 2),
STCTRL = (0x010 >> 2),
STRELOAD = (0x014 >> 2),
STCURRENT = (0x018 >> 2),
PRI3 = (0xD20 >> 0)
};
void pll(void){
uint32_t tmp;
SYSCTL[SYSCTL_MOSCCTL] &= ~(SYSCTL_MOSCCTL_NOXTAL | SYSCTL_MOSCCTL_PWRDN);
if (!(SYSCTL[SYSCTL_MOSCCTL] & SYSCTL_MOSCCTL_OSCRNG)){
SYSCTL[SYSCTL_MOSCCTL] |= SYSCTL_MOSCCTL_OSCRNG;
while (!(SYSCTL[SYSCTL_RIS] & SYSCTL_RIS_MOSCPUPRIS));
}
SYSCTL[SYSCTL_MISC] = SYSCTL_MISC_MOSCPUMIS;
SYSCTL[SYSCTL_RSCLKCFG] |= SYSCTL_RSCLKCFG_OSCSRC_MOSC | SYSCTL_RSCLKCFG_PLLSRC_MOSC;
SYSCTL[SYSCTL_PLLFREQ0] = (96 << SYSCTL_PLLFREQ0_MINT_S) | (0 << SYSCTL_PLLFREQ0_MFRAC_S);
SYSCTL[SYSCTL_PLLFREQ1] = 4;
tmp = SYSCTL[SYSCTL_MEMTIM0];
tmp &= ~(SYSCTL_MEMTIM0_EBCHT_M | SYSCTL_MEMTIM0_EWS_M | SYSCTL_MEMTIM0_EBCE);
tmp |= SYSCTL_MEMTIM0_FBCHT_3_5 | SYSCTL_MEMTIM0_EWS_6;
tmp &= ~(SYSCTL_MEMTIM0_FBCHT_M | SYSCTL_MEMTIM0_FWS_M | SYSCTL_MEMTIM0_FBCE);
tmp |= SYSCTL_MEMTIM0_FBCHT_3_5| SYSCTL_MEMTIM0_FWS_6;
SYSCTL[SYSCTL_MEMTIM0] = tmp;
SYSCTL[SYSCTL_PLLFREQ0] |= SYSCTL_PLLFREQ0_PLLPWR;
SYSCTL[SYSCTL_RSCLKCFG] |= SYSCTL_RSCLKCFG_NEWFREQ;
while (!SYSCTL[SYSCTL_PLLSTAT]);
tmp = SYSCTL[SYSCTL_RSCLKCFG];
tmp = (tmp & ~SYSCTL_RSCLKCFG_PSYSDIV_M) | SYSCTL_RSCLKCFG_PSYSDIV_3;
tmp |= SYSCTL_RSCLKCFG_USEPLL | SYSCTL_RSCLKCFG_MEMTIMU;
SYSCTL[SYSCTL_RSCLKCFG] = tmp;
}
unsigned long piano(void){
unsigned long freq;
if (!GPIO_PORTK[IN_PK4]){
freq = C;
GPIO_PORTN[LED1_PN1] ^= LED1_PN1;
}
else if(!GPIO_PORTK[IN_PK5]){
freq = D;
GPIO_PORTN[LED2_PN0] ^= LED2_PN0;
}
else if(!GPIO_PORTK[IN_PK6]){
freq = E;
GPIO_PORTF[LED3_PF4] ^= LED3_PF4;
}
else if(!GPIO_PORTK[IN_PK7]){
freq = G;
GPIO_PORTF[LED4_PF0] ^= LED4_PF0;
}
else
freq = 0;
return freq - 1;
}
void DAC(unsigned long data){
if (GPIO_PORTK[in] != in)
GPIO_PORTK[out] = 0;
else
GPIO_PORTK[out] = data;
}
void tone(unsigned long period){
SysTick[STRELOAD] = period;
}
void sysHand(void){
index = (index + 1) & 0x30;
DAC(sin[index]);
}
void main()
{
pll();
SysTick[STCTRL] = 0;
SysTick[STCURRENT] = 0;
SysTick[PRI3] = (0x2 << 28);
SysTick[STCTRL] = 0x7;
SysTick[STRELOAD] = 1000000;
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTN;
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTF;
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTJ;
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTK;
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTN;
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTF;
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTJ;
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTK;
GPIO_PORTN[GPIO_DIR] |= LED1_PN1;
GPIO_PORTN[GPIO_DEN] |= LED1_PN1;
GPIO_PORTN[GPIO_DIR] |= LED2_PN0;
GPIO_PORTN[GPIO_DEN] |= LED2_PN0;
GPIO_PORTF[GPIO_DIR] |= LED3_PF4;
GPIO_PORTF[GPIO_DEN] |= LED3_PF4;
GPIO_PORTF[GPIO_DIR] |= LED4_PF0;
GPIO_PORTF[GPIO_DEN] |= LED4_PF0;
GPIO_PORTJ[GPIO_PUR] |= PUSH1_PJ0 | PUSH2_PJ1;
GPIO_PORTJ[GPIO_DEN] |= PUSH1_PJ0 | PUSH2_PJ1;
GPIO_PORTK[GPIO_DIR] &= ~in;
GPIO_PORTK[GPIO_DEN] |= in;
GPIO_PORTK[GPIO_DIR] |= out;
GPIO_PORTK[GPIO_DEN] |= out;
while(true){
GPIO_PORTN[LED1_PN1] ^= LED1_PN1;
}
}
#include <stdint.h>
#include <stdbool.h>
#define GPIO_PORTA ((volatile uint32_t *)0x40058000)
#define SYSCTL ((volatile uint32_t *)0x400fe000)
#define SysTick ((volatile uint32_t *)0xE000E000)
#define GPIO_PIN_3 (1 << 3)
#define GPIO_PIN_4 (1 << 4)
#define GPIO_PIN_5 (1 << 5)
#define SYSCTL_RCGCGPIO_PORTA (1 >> 0)
#define left GPIO_PIN_5
#define right GPIO_PIN_4
#define button GPIO_PIN_3
#define SYSCTL_MOSCCTL_PWRDN (1 << 3)
#define SYSCTL_MOSCCTL_NOXTAL (1 << 2)
#define SYSCTL_MOSCCTL_OSCRNG (1 << 4)
#define SYSCTL_RIS_MOSCPUPRIS (1 << 8)
#define SYSCTL_MISC_MOSCPUMIS (1 << 8)
#define SYSCTL_RSCLKCFG_OSCSRC_MOSC (3 << 20)
#define SYSCTL_RSCLKCFG_PLLSRC_MOSC (3 << 24)
#define SYSCTL_RSCLKCFG_NEWFREQ (1 << 30)
#define SYSCTL_RSCLKCFG_PSYSDIV_M (0x3ff >> 0)
#define SYSCTL_RSCLKCFG_PSYSDIV_3 3
#define SYSCTL_RSCLKCFG_USEPLL (1 << 28)
#define SYSCTL_RSCLKCFG_MEMTIMU (1 << 31)
#define SYSCTL_PLLFREQ0_MINT_S 0
#define SYSCTL_PLLFREQ0_MFRAC_S 10
#define SYSCTL_PLLFREQ0_PLLPWR (1 << 23)
#define SYSCTL_MEMTIM0_EBCHT_M (0b1111 << 22)
#define SYSCTL_MEMTIM0_EWS_M (0b1111 << 16)
#define SYSCTL_MEMTIM0_EBCE (1 << 21)
#define SYSCTL_MEMTIM0_FBCHT_3_5 (6 << 6)
#define SYSCTL_MEMTIM0_EWS_6 (6 << 16)
#define SYSCTL_MEMTIM0_FBCHT_M (0b1111 << 6)
#define SYSCTL_MEMTIM0_FWS_M (0b1111 >> 0)
#define SYSCTL_MEMTIM0_FBCE (1 << 5)
#define SYSCTL_MEMTIM0_FWS_6 (6 >> 0)
#define TOGGLE_OFF 0
#define TOGGLE_ON 1
enum {
SYSCTL_RCGCGPIO = (0x608 >> 2),
GPIO_DEN = (0x51c >> 2),
GPIO_DIR = (0x400 >> 2),
SYSCTL_MOSCCTL = (0x07C >> 2),
SYSCTL_RIS = (0x050 >> 2),
SYSCTL_MISC = (0x058 >> 2),
SYSCTL_RSCLKCFG = (0x0B0 >> 2),
SYSCTL_PLLFREQ0 = (0x160 >> 2),
SYSCTL_PLLFREQ1 = (0x164 >> 2),
SYSCTL_MEMTIM0 = (0x0C0 >> 2),
SYSCTL_PLLSTAT = (0x168 >> 2),
STCTRL = (0x010 >> 2),
STRELOAD = (0x014 >> 2),
STCURRENT = (0x018 >> 2),
PRI3 = (0xD20 >> 0)
};
void pll(void){
uint32_t tmp;
SYSCTL[SYSCTL_MOSCCTL] &= ~(SYSCTL_MOSCCTL_NOXTAL | SYSCTL_MOSCCTL_PWRDN);
if (!(SYSCTL[SYSCTL_MOSCCTL] & SYSCTL_MOSCCTL_OSCRNG)){
SYSCTL[SYSCTL_MOSCCTL] |= SYSCTL_MOSCCTL_OSCRNG;
while (!(SYSCTL[SYSCTL_RIS] & SYSCTL_RIS_MOSCPUPRIS));
}
SYSCTL[SYSCTL_MISC] = SYSCTL_MISC_MOSCPUMIS;
SYSCTL[SYSCTL_RSCLKCFG] |= SYSCTL_RSCLKCFG_OSCSRC_MOSC | SYSCTL_RSCLKCFG_PLLSRC_MOSC;
SYSCTL[SYSCTL_PLLFREQ0] = (96 << SYSCTL_PLLFREQ0_MINT_S) | (0 << SYSCTL_PLLFREQ0_MFRAC_S);
SYSCTL[SYSCTL_PLLFREQ1] = 4;
tmp = SYSCTL[SYSCTL_MEMTIM0];
tmp &= ~(SYSCTL_MEMTIM0_EBCHT_M | SYSCTL_MEMTIM0_EWS_M | SYSCTL_MEMTIM0_EBCE);
tmp |= SYSCTL_MEMTIM0_FBCHT_3_5 | SYSCTL_MEMTIM0_EWS_6;
tmp &= ~(SYSCTL_MEMTIM0_FBCHT_M | SYSCTL_MEMTIM0_FWS_M | SYSCTL_MEMTIM0_FBCE);
tmp |= SYSCTL_MEMTIM0_FBCHT_3_5| SYSCTL_MEMTIM0_FWS_6;
SYSCTL[SYSCTL_MEMTIM0] = tmp;
SYSCTL[SYSCTL_PLLFREQ0] |= SYSCTL_PLLFREQ0_PLLPWR;
SYSCTL[SYSCTL_RSCLKCFG] |= SYSCTL_RSCLKCFG_NEWFREQ;
while (!SYSCTL[SYSCTL_PLLSTAT]);
tmp = SYSCTL[SYSCTL_RSCLKCFG];
tmp = (tmp & ~SYSCTL_RSCLKCFG_PSYSDIV_M) | SYSCTL_RSCLKCFG_PSYSDIV_3;
tmp |= SYSCTL_RSCLKCFG_USEPLL | SYSCTL_RSCLKCFG_MEMTIMU;
SYSCTL[SYSCTL_RSCLKCFG] = tmp;
}
struct state{
unsigned int out;
unsigned int next[2];
}; typedef const struct state fsm;
fsm sound[2] = {
{0, {TOGGLE_OFF, TOGGLE_ON}},
{1, {TOGGLE_ON, TOGGLE_OFF}}
};
unsigned int input = 0;
unsigned int output = 0;
unsigned int curr = TOGGLE_OFF;
void sys_hand(void){
if (output == 1){
GPIO_PORTA[left] ^= left;
GPIO_PORTA[right] ^= right;
} else if((output == 0) && (GPIO_PORTA[button] == 0x00)){
GPIO_PORTA[left] = 0;
GPIO_PORTA[right] = 0;
} else{
GPIO_PORTA[left] = 0;
GPIO_PORTA[right] = 0;
}
}
void delay(unsigned int param){
unsigned int i, j;
for(j = 0; j < param; j++){
for(i = 0; i < 15; i++){
}
}
}
void edgeDetect(char param){
if (param == 'r'){
output = sound[curr].out;
if (GPIO_PORTA[button] == 0){
delay(1);
if (!GPIO_PORTA[button])
input = TOGGLE_ON;
} else
input = TOGGLE_OFF;
curr = sound[curr].next[input];
}
else if (param == 'f'){
output = sound[curr].out;
if (!GPIO_PORTA[button]){
delay(1);
if (GPIO_PORTA[button] == 0)
input = TOGGLE_ON;
} else
input = TOGGLE_OFF;
curr = sound[curr].next[input];
}
}
void main(void)
{
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTA;
SYSCTL[SYSCTL_RCGCGPIO] |= SYSCTL_RCGCGPIO_PORTA;
GPIO_PORTA[GPIO_DEN] |= button;
GPIO_PORTA[GPIO_DIR] &= ~button;
GPIO_PORTA[GPIO_DIR] |= left;
GPIO_PORTA[GPIO_DEN] |= left;
GPIO_PORTA[GPIO_DIR] |= right;
GPIO_PORTA[GPIO_DEN] |= right;
SysTick[STCTRL] = 0;
SysTick[STRELOAD] = 136363;
SysTick[STCURRENT] = 0;
SysTick[PRI3] = (0x2 << 28);
SysTick[STCTRL] = 0x7;
pll();
while(true){
edgeDetect('r');
sys_hand();
}
}
Could you help look into it? Thank you for your help.