Part Number: AM2432
Hi team,
In my previous thread I asked a question on different encoder firmware, listed as below.
Q: AM243X supports BISS-C, ENDAT and TAMAGAWA encoders, but is it supported to use the same pins? That is, the fixed pins of the processor are connected to RS485, and the switching of the above three encoder functions can be realized through software settings?At present, in our products, the above three encoder interface functions are implemented in the FPGA. When the interface function is switched, there is no need to change the hardware circuit.
A: [MW] Yes and No. The hardware pin mux may not change when you switch the encoder protocol, but the PRU-ICSSG firmware will need to change, because different encoder protocol uses different PRU-ICGGS firmware and the encoder driver is different too.
Since my customer has no experience on this topology, could you please suggest what steps they should follow? An instruction is preffered, many thank!
BR
Sirui