Part Number: AM2431
The spruj63.pdf, EVM User’s Guide, Section 3.3, describes the powerOn/Off Procedures for one EVM.
- What is the procedure regarding power when two EVMs,one as a root complex & the other as an endpoint, are connected using a PCIe cable between the two PCIe sockets?
- Is 12V power only applied to the root complex EVM?
- With 3.3V supplied on both EVMs, what is the method that should be used to isolate these two supplies?
- Is there a document that provides information on connecting two Sitara EVMs together with a male to male PCIe cable?