Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Hi Experts,
I am asking for my customer.
Customer are using DDR based on LP-AM423, and they refer the below step and customer do not know how to modify this.
1. Go to https://dev.ti.com/sysconfig/?product=Processor_DDR_Config&device=AM243x_beta and add a new DDR4 instance:
2. Use the generated AM243x-DDRConfig.gel to replace the C:\ti\ccs1200\ccs\ccs_base\emulation\gel\AM24x\AM24_DDRSS\AM24x-DDR4-1600MTs.gel
3. re-run the load_dmdsc.js and the AM2434_EVM DDR script.
You can also adjust the following:
1. DDR Memory Type
2. System Configuration
3. DRAM Timing A/B
4. IO Control A/B
Could you help to provide the board_ddrReginit.h, GUI Sysconfig configuration interface of DDR on EVM board?
The DDR4 chip used by the customer is MT40A512M16-62E:R
The DDR4 chip of the EVM is MT40A1G16KD-062EIT:E.
Customers want to directly refer to the Sysconfig configuration parameters on the EVM board to make corresponding modifications? Could you support this case? Or is it possible to provide oard_ddrReginit.h based on customer's DDR chip? Thanks.