Hello,
we are using MCU Plus SDK 08.04 without the new flash-driver since there is still an issue with ISSI-Flashes we are working on with TI. We are also using different flashes on our pcbas. The correct flash is identified by its id on startup and the matching configurations are then loaded. So currently there can be an ISSI or an Gigadevice (GD25LX256E)-Flash.
The ISSI-Flashes work with PHY-mode but the Gigadevice-Flashes do not properly. At least that's our first assumption. It may also occur now because we got some new charges of AM2434-Sitara SoCs which are used with the combination of the GigaDevice-Flash.
We noticed that at Boot-time, when booting from Flash the Flash_read-commands in our SBL return with Success but the read data is not correct. This happens randomly sometimes. Like in 20% of the power-ups.
This does not happen with the ISSI-Flash. We set the configuration of the Gigadevice-flash according to its data sheet. Also the RBL does work, and the read-id-command in 1s-1s-1s-mode also works. Also setting it to OCTAL SPI works but then using the PHY-Mode seems to break the operation.
The speed is set to 200 MHz or to 133 Mhz, in both cases the problem occurs, when the PHY is enabled. When PHY is disabled the problem does not occur.
We have 1k Pull-Down connected to DQS, which should be suitable.
To catch the issue I inserted a while-loop in our SBL-code when the read data is not correct. Interestingly when I connect via CCS the memory browser shows the correct data inside the flash and if I trigger a read-operation (so jumping to the read-operation in CCS and execute it) it suddenly reads the correct data.
I thought as a temporary workaround that maybe a sleep would then provoke the correct behaviour but even a 200 ms-sleep after Flash_open still does not help.
I saw there is a big file for PHY-tuning. Does this take care of the mentioned bug of the PHY-mode in the errata (i2189)?
Since our SBL uses sensitive data which is important for booting which is located inside the flash, a wrong read would lead to a fallback and the correct fw which should be booted is not booted anymore. This will mean that from now on produced devices will end in a non-useable state for our customers. This is a blocking point for us.
As a workaround we can disable the PHY-mode, but that would mean we would only run with 50 MHz. And we also noticed that the read-operations will take much longer. This would slow the application since we also use a webserver which needs flash-access and a file-system and so on.
Best regards
Felix