Part Number: TMDSEMU110-U
Other Parts Discussed in Thread: UNIFLASH
Hello Support,
Working on a project where I need to flash more than 10 microcontrollers in the same product, I'm using the following configuration:
- computer used for this project runs on Windows 7 (64 bits),
- TI_Debug_Probe USB driver (2.0.0.2) has been installed thanks to a standalone package made with UniFlash 8.0 tool,
- one XDS110 probe per target,
- each XDS110 probe has been updated to 3.0.0.20 firmware,
- two USB HUB (with external power supply) are chained to reach the total required number of USB connectors for the XDS110 probes.
Having a script to make programmation of the whole product faster, I'm facing an issue when the number of connected XDS110 is greater than 9 probes. Windows Device Manager always returns a code 10 error (CM_PROB_FAILED_START) on the 10th connected probe whichever probe is the 10th to be connected on any of the two USB HUB.
Could you please tell me if there is any limitation on how many XDS110 probe could be connected on the same computer?
Is there any more up-to-date driver which could handle such configuration?
If not, do you have any suggestion to handle a USB power up / power down sequence with some Windows / custom TI tool commands?
Thanks in advance,
Best Regards,
Adrien.