Dear TI support,
I would like to know more regarding the data flash memory write/erase cycles. I'm aware that the flash can withstand 100000 cycles as specified in the datasheet (see picture below). However I would to know if you have more data regarding this topic, mainly:
- What exactly happens when we pass the maximum number of cycles? Is the processor going to detect a problem and never start again ?
- Can the processor eventually detect this type of problems?
- Is there a register that counts the number of writes/Erases during it's lifetime?
- Do you have any statistical data ? For example 10 out 100 processors will fail after this number of cycles
- How is the this number affected by the years ? Is the maximum number of write/erase cycles the same weather I use the processor for 5 years of for 15 years?
Thanks,