This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Question about multiple HR instructions in N2HET

Part Number: TMS570LC4357

reference to SPNA178 – April 2015: Monitoring PWM Using N2HET

In the PWM monitoring N2HET program,

Both

L02 PCNT { hr_lr=HIGH,type=RISE2FALL,pin=PULSE_MONITOR_PIN_NUM};

and

L04 MCMP {
next=L00,hr_lr=LOW,cond_addr=L05,pin=0,order=REG_GE_DATA,reg=R,data=SKIP_EDGES,hr_data=0};

Can MCMP also uses hr_lr = HIGH when MCMP(pin) is different from PCNT(pin) ? To my understanding, in one loop, only one HR instruction in HR mode for each N2HET PIN can be used, so multiple HR Instructions with different PINs are allowed ?

Is this correct ?