Part Number: EK-TM4C123GXL
After a timer is disabled. I want to switch the configured pin also off.
How i can do this?
Because when i start both timers again. I want to start in a preconfigured state.
void init_TIMER_0()
{
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
while(!MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_TIMER0));
// Timer 0A is the data signal 1: PB6
// Timer 0B is the udma trigger signal to GPIO: PB7
MAP_GPIOPinConfigure(GPIO_PB6_T0CCP0);
MAP_GPIOPinConfigure(GPIO_PB7_T0CCP1);
MAP_GPIOPinTypeTimer(GPIO_PORTB_BASE, GPIO_PIN_6);
MAP_GPIOPinTypeTimer(GPIO_PORTB_BASE, GPIO_PIN_7);
MAP_TimerConfigure(TIMER0_BASE, TIMER_CFG_SPLIT_PAIR |
TIMER_CFG_A_PWM | TIMER_CFG_B_PWM);
MAP_TimerLoadSet(TIMER0_BASE, TIMER_BOTH,
(SysCtlClockGet()/SIGNAL_FREQUENZ) - 1);
// start led signal with the reset signal
MAP_TimerMatchSet(TIMER0_BASE, TIMER_A, SIGNAL_RESET);
// DMA Request
MAP_TimerMatchSet(TIMER0_BASE, TIMER_B, SIGNAL_DMA);
}