Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Question about extending flash and sdram through emif

Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN

Hi Team,

My customer has two questions about TMS570LC4357 emif extension:

1. For the external NOR FLASH, after I configure the CEnCFG register according to the requirements of TRM during initialization, how should I read, write and erase the FLASH? Is it to operate through the F021 API like the internal FLASH or directly read and write through the address? Are there any relevant routines that can be referred to?

2. For the external SDRAM, can I read and write it after I configure it according to Procedure A or Procedure B given in the chapter 21.2.5.5 SDRAM Configuration Procedure in TRM? Can it be manipulated directly by physical address?

--

Thanks & Regards

Yale