Hello,
I am using CCS 12 and would like to add the ecat beckhoff slave demo project into git via Microsoft Azue. I followed instructions and am able to add the project files such as makefile etc into the git repo but not sdk files for some reason. I tried manually to add them into the git via "Team" but I did not see the "Add" index meanu. These sdk files are in the original example folder. Please help.
Thanks.
Ming