Part Number: MSPM0G1106
Other Parts Discussed in Thread: LM4040
I am looking to use 8 of the ADC pins for measuring voltages.
1) in terms of accuracy it seems that an external reference helps a little bit. I was wondering if you could quantify how much each of these could help and make a recommendation.
a) using an external reference, VREF+ only
b) using an external reference, using VREF+ and -
c) using an external reference of 3V instead of 2.5V
d) I do have the ability to generate an external 3.3V reference from 5V, different than the 3.3V VCC, but I wasn't sure if that was going to cause any troubles if the ref were above vcc, or how much it would help
2) If i'm using an external reference, can you advise? i'm not in a power critical design. I would like something that will not likely have supply issues.
the LM4040 seemed like a good starting point, but its an older part. Should i be looking at a different family? you have many LM, REF parts which can do the job.
thanks.