Part Number: TMS570LC4357
Will the protrace able to support the RAM Trace Port RTP?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Will the protrace able to support the RAM Trace Port RTP?
Hi Deric,
RTP is used to trace all accesses to the internal RAM or peripherals without impacting the CPU's code execution. ETM is used to trace the execution of the main Cortex-R5F processor. They use different MCU pins.
The XDS Trace Pro doesn't support RTP.
Hi Jagadish
Thanks, can you recommend any tools that can perform the RTP? I saw that the HDK board consists of the both Mipi60 and 38pin connector. Can i run the protrace and RTP debugger at the same time?
Please check Vector VX1000.
run the protrace and RTP debugger at the same time?
RTP signal pins are not multiplexed with ETM signals. They can run at the same time.