Part Number: MSPM0L1105
MSP team,
We have a customer working with MSPM0L1105TDYYR (16 pin SOT DYY). They have an I2C port with pull-ups on it. They need to disable power completely to the device during shutdown, but the pull-ups for I2C will still have a voltage applied (eg. 3.3V).
Based on section 7.1 of the datasheet, it looks like this is fine, since the Abs Max is not dependent on VDD. This is assuming they use the 5V tolerant IO, pins 3 and 4.
Can you confirm this is correct?
Thanks,
Darren