Part Number: LP-AM243
Other Parts Discussed in Thread: DP83869
Hi Experts,
I am using the enet_lwip_cpsw example from MCU+SDK 08.05.00.24 on the lp-am243. It is running as expected using DHCP, but only if I disable the second netif.
However, I want to use a static IP address. So I changed
--- lwipcfg.h
#define LWIP_PORT_INIT_IPADDR(addr) IP4_ADDR((addr), 192,168,39,5)
#define LWIP_PORT_INIT_GW(addr) IP4_ADDR((addr), 192,168,39,1)
#define LWIP_PORT_INIT_NETMASK(addr) IP4_ADDR((addr), 255,255,255,0)--- lwipopts.h
#define LWIP_DHCP 0
This used to work with the previous SDK.
However, in this case the firmware runs into a RTOS abort.
Is this a bug, or is there a different way to use a static IP address? Which documentation should I look in?
Thanks for a hint
Alexander

2063.enet_lwip_cpsw_am243x-lp_r5fss0-0_freertos_ti-arm-clang.zip