Part Number: AM2432
Other Parts Discussed in Thread: UNIFLASH
Hi team,
My customer has issue on SBL burning via UART. Below is the debug info. Could you have a look on this issue?
PS C:\ti\mcu_plus_sdk_am243x_08_05_00_24\tools\boot> python uart_uniflash.py -p COM3 --cfg=sbl_prebuilt/am243x-lp/default_sbl_null.cfg
Parsing config file ...
Parsing config file ... SUCCESS. Found 2 command(s) !!!
Executing command 1 of 2 ...
Found flash writer ... sending sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage
Sent flashwriter sbl_prebuilt/am243x-lp/sbl_uart_uniflash.release.tiimage of size 294772 bytes in 27.38s.
Executing command 2 of 2 ...
Command arguments : --file=sbl_prebuilt/am243x-lp/sbl_null.release.tiimage --operation=flash --flash-offset=0x0
Sending sbl_prebuilt/am243x-lp/sbl_null.release.tiimage: 0%| | 0/258683 [00:00<?, ?bytes/s]send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'2'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'1'
send error: expected NAK, CRC, EOT or CAN; got b'1'
Sending sbl_prebuilt/am243x-lp/sbl_null.release.tiimage: 0%| | 2/258683 [00:01<143:34:46, 2.00s/bytes]
[ERROR] XMODEM send failed, no response OR incorrect response from EVM OR cancelled by user,
Power cycle EVM and run this script again !!!
PS C:\ti\mcu_plus_sdk_am243x_08_05_00_24\tools\boot>
BR
Sirui