Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: MSPM0G3507
Hi
I looking into using OpenOCD for debugging against (to begin with) the LP-MSPM0G3507.
To get OpenOCD to work it needs a couple of config files, there already exist a config file for the interface/debugger XDS110,
but it also need one (or two) representing the target and board.
I have tried to look into what's needed to create a board/target config, but to be honest, it's a bit a bit over my head.
So wondering if someone has already gotten OpenOCD to work with LP-MSPM0G3507?
Or at least any hints on how to create the board/target config?
There exist configs for the MSP432, would it be possible to modify them to get it to work with the MSPM0G3507?