Part Number: AM2634
Other Parts Discussed in Thread: SYSCONFIG
Dear Champs,
Could you please clarify what is maximum baud-rate of UART in AM2634?
Is it possible to achieve 12Mbps or 3.6Mbps baud-rate of UART in AM2634?
I found only 16x mode UART(<= 115.2kbaud/s) is supported in current MCU+SDK(v8.5.0) as below.
So, I would like to check if this is right and there is any way to implement over 115.2kbps baud-rate in UART.
And also, I would like to check if we have a plan to support RS485 and 10Mbps baud-rate of UART in AM2634 in future.
Thanks and Best Regards,
SI.