Part Number: MSPM0L1306
HI,
What can I do to speed up the A/D Conversion time?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Anjli,
What sample rate are you targeting? Take a look at the adc12_max_freq_dma_LP_MSPM0L1306 example in the SDK. This example configure the MSPM0L for the maximum sampling rate.
Things like your conversion resolution, sample time settings, and trigger source can determine your overall sample rate.
Best Regards,
Brandon Fisher
For this response, I'm referencing both the device datasheet and Technical Reference Manual (TRM).
There are three components that will drive the total conversion time.
The TRM has a diagram of this sequence in section 9.2.9.1.
Trigger
Has a minimum of 3 ADCCLK cycles for software trigger. For hardware trigger sources, this will be 2 or 3 ADCCLK cycles.
Sample Time
You can see from table in the datasheet section 7.12.2 different proposed sampling times under different source conditions to the ADC. Essentially what matters is the external drive strength capability into the ADC, and this is design dependent. If you know your source characteristics, you can calculate the sample time you need based on the datasheet section 7.12.1 specification of a 4pF sample-and-hold cap with 0.5k ohm series resistance. You also need to account for the pin capacitance (CI). This is basic RC time constant math. The datasheet section 7.12.4 has a nice diagram of the internal circuitry of ADC to help you visualize this.
The sample period is adjusted by the SAMPCLK bits of the ADC CLKCFG register, as described in the TRM section 9.2.9. If you are not getting an accurate ADC conversion result, a common root cause is too short of a sample period.
Conversion Time
Conversion time is dependent on the configured resolution and CONVCLK clock frequency (TRM section 9.2.3):
To adjust the CONVCLK, derived from ADCCLK, see TRM section 9.2.5. Possible clock sources are ULPCLK and SYSOSC, chosen by the SMPCLK field of the ADC CLKCFG register. You will also want to take care to adjust the ADC CLKFREQ register based on the chosen clock settings. You do need to be aware of your reference source. if the internal reference is used, the maximum conversion clock frequency must not exceed 4MHz.
Thanks,
Stuart