Part Number: MSP432E401Y
Other Parts Discussed in Thread: TM4C123GH6PZ
Hi,
I am trying to use two ADCs of MSP432E401Y for sampling I-Q two channels simutaneously, and I want to know if the two ADCs can be trigered with the saem trigger source.
In TM4C123GH6PZ datasheet, page 813, it was clearly said "The trigger source for ADC0 and ADC1 may be independent or the two ADC modules may operate from the same trigger source and operate on the same or different inputs." But in the datasheet of MSP432E401Y, I did not find similar description. So I want to make sure, I can use the two ADC in MSP432E401Y for sampling I-Q channels.
Tahnk you very much,
Zhonghai