Part Number: PRU-SWPKG
Other Parts Discussed in Thread: BEAGLEBOARD-X15
Hi
In Windows 10 Pro, I'm trying to run the example program for PRU core in Beagleboard-x15. I used the ready image "tisdk-base-image-am57xx-evm.tar.xz" from TI linux SDK "ti-processor-sdk-linux-am57xx-evm-08_02_01_00". Then, i tried the "PRU_Halt" from "pru-software-support-package-6.1.0" and include files from "pru-icss-6.0.1".
Then followed the section "Create & Build the PRU Project" and code builds successfully. The remoteproc module also enabled in the kernel
I load the firmware("PRU_Halt.out") in path "/lib/firmware/pru" and ran using the below command
echo 'pru/PRU_Halt.out' > /sys/class/remoteproc/remoteproc1/firmware
echo 'start' > /sys/class/remoteproc/remoteproc1/state
But it shows the error
root@am57xx-evm:/lib/firmware/pru# echo 'start' > /sys/class/remoteproc/remoteproc1/state
-sh: echo: write error: Invalid argument
[ 3263.741455] remoteproc remoteproc1: powering up 55020000.ipu
[ 3263.741607] remoteproc remoteproc1: Booting fw image pru/Tr1PRU.out, size 22448
[ 3263.741668] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 3263.741729] remoteproc remoteproc1: Boot failed: -22
I tried the different program and example but it's not booting.
The details are
IDE: CCS v12.3.0.00005
Compiler version: ti_cgt_pru_2.3.3
Beagleboard-x15 os: Arago 2021.09 with Linux am57xx-evm 5.10.100-rt62-g204ec708dc #1 SMP PREEMPT_RT
The question is releated to another question (click here)
Let me know the suggestion.