Hello TI team,
I would like to know what is the maximum component height on top and bottom side of the Launchpad LP-AM243. Could you please check?
regards,
Biju
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Biju,
I assume you are asking about components outside of the boostpack headers, correct?
For the top of the board, the ethernet jacks are far and away the tallest component at 13.45mm to the body (note that the tabs stick a little higher than this). Next would be USB Type C connector at 2.96mm, the USB Type B connector at 2.66mm. For components, the tallest are U2,the QSPI flash, and SW4, the dip switches at 2.5mm each.
For the bottom of the board, all the surface mount components are pretty similar in height, with the tallest being a little over 1mm. The alignment pegs for the ethernet jacks actually stick out further from the board at just over 2mm.
Let me know if this sufficiently answers your question.
Thanks,
Mike