Part Number: LP-AM243
Other Parts Discussed in Thread: AM2434
Hi TI team,
Whether LP-AM243 support USB OTG feature?
regards,
Biju
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Biju,
While the devices are capable of supporting USB OTG, we do not have that functionality included as part of the LP-AM243 nor do we have example code for OTG with our SDK.
To support USB OTG you'd need to use the USB0 ID as part of the Host Negotiation Protocol. The LaunchPad does not have this pin brought out to the USB connector and the current configuration for USB0 ID is to leave it floating which means that the AM2434 would be operating in device mode for USB 2.0.
Best Regards,
Ralph Jacobi