I think i have connected the L+ and L- wires wrongly with the CQ line and due to which the Nfault LED is always on and the VCC out is only giving me 2.4V instead of 5V.
All the other LED's are now very dim as compared to earlier when they were lit brightly.
Is the device now spoilt ? how can i diagnose the Nfault error ?