Part Number: TMDSEMU110-U
We recently purchased 3 of the XDS110 Debug probes to program some TI-C2000 based DSP boards we had made. Since ribbon cables and connectors are notoriously fragile, I was hoping to purchase some extras of both the 20 pin JTAG cables and 14 pin AUX cables, but I couldn't find them available on you website. Is it possible to order these? (If not, could you supply me the connector particulars, and I will see about getting them from another source, like Molex etc.)
Also, it looks like we will have to make a custom adapter f to use the AUX capabilities; is there a 12 pin connector that mates with the supplied AUX breakout adapter?