Hello,
Here are two questions that have been discussed with TI over the call. I just create this thread to track the status.
- To understand whether it is possible to leverage ESM reset status register to indicate watchdog reset has occurred. With several SW warm reset use case, need to figure out a way to identify watchdog reset to increase watchdog reset counter.
- To understand whether it is feasible to set the r5f core0’s watchdog timer reset expiration time to be 3/5 minutes for SBL bootloader, and re-configures the same watchdog timer with a longer expiration time for appimage. The current appimage uses 70 minutes expiration time, which would need to increase a counter 5 times. TI would explore the possibility to eliminate the use of the counter.
Thanks,
Hong