Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
I'm using ADC triggered from PWM SOCA, not in Continuous Conversion mode.
I got HALCoGen setup here

generated code like this
uint32 adcGetData(adcBASE_t *adc, uint32 group, adcData_t * data)
{
uint32 i;
uint32 buf;
uint32 mode;
uint32 index = (adc == adcREG1) ? 0U : 1U;
uint32 intcr_reg = adc->GxINTCR[group];
uint32 count = (intcr_reg >= 256U) ? s_adcFiFoSize[index][group] : (s_adcFiFoSize[index][group] - (uint32)(intcr_reg & 0xFFU));
adcData_t *ptr = data;
/* USER CODE BEGIN (16) */
/* USER CODE END */
During code execution, I got somewhere count is actual negative results:

So why is this? is it a bug or I should just access ADC results directly from ADC buffer instead?
thanks