This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: Problem with ethernet connection initialization in TI RTOS for TM4C1294

Part Number: TM4C1294NCPDT

Hello,

I have seen that when I connect the ethernet cable to TM4C1294 and when connection is being initialized, all other tasks (including critical HWI tasks) stall for 200-300 ms. Is this related to netHook priority or something else.

Also, after I perform, for example, 5th connection, microcontroller stops making connections, even if I connect the TM4C to the same PC (by connecting and disconnecting the same ethernet cable). I suppose that this is related to the maximum connections parameters. Is it possible to redirect the connection to existing hooks, since the connection is being made to the same PC.

Regards