Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hello
Regarding the control of special multiplexed options for eCAPx, there are discrepancies between the documents SPNS195C (JUNE 2016) in "Table 7-8. Device-Level Input Connection to eCAPx Modules" and SPNU563A (March 2018) in "Table 6-8. Controls for eCAPx Inputs" of the TMS570LC43x for the setting of PINMMR169 and PINMMR170.
Is the correct setting for using the double-VCLK3-synchronised input with no filter 01b respectively bits 0, 8, 16, 24 are set to 1, e.g. PINMMR169[1:0] = 01 analogoue to eQEPx modules (e.g. PINMMR170[17:16] = 01)?
Thanks in advance for the support
Mathieu