Part Number: RM44L920
I am using eCAP module in continous capture mode,i found that at some times the two event capture values are same (C1:11539,c2:11539,c3:93510,c4:331453) c1,c2c,3c,c4 are the capture event values.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: RM44L920
I am using eCAP module in continous capture mode,i found that at some times the two event capture values are same (C1:11539,c2:11539,c3:93510,c4:331453) c1,c2c,3c,c4 are the capture event values.
Hi Karthik,
I am using eCAP module in continous capture mode,i found that at some times the two event capture values are same (C1:11539,c2:11539,c3:93510,c4:331453) c1,c2c,3c,c4 are the capture event values.
Why it can't be same? It might coincidence, right?
what signals are you capturing?
--
Thanks & regards,
Jagadish.
Hi Karthik,
I am using eCAP module in continous capture mode,i found that at some times the two event capture values are same
The only thing i am suspecting is that,

As you can see that minimum pulse width for capture should be 2 times of the VCLK3 period right. In your case if the pulse width between the capture event-1 and capture event-2 is less than this required pulse width then before the counter increment to the next value you will get capture the two periods for event-1 and event-2 and in this case both captures would be the same values.
--
Thanks & regards,
Jagadish.
Hi Jagadish,
I understood what you say,but if the two eCAP capture values are same then how am i supposed use those values if i need four pulses to calculate speed .Is there any alternate way to get the 4 eCAP values correctly without same value?
Hi Karthik R,
Sorry the last screenshot is from another datasheet not from RM44L920, just now i checked in RM44L920 datasheet and there i found it is depends on VCLK4 instead of VCLK3.

Is there any alternate way to get the 4 eCAP values correctly without same value?
Can you please try by increasing VCLK4 frequency once?

I don't know what value you configured for VLCK4 in your application and it can be max of 150MHZ. So, try with this max value and see the capture values. If we increase the VCLK4 frequency then it can capture high frequencies as well.
--
Thanks & regards,
Jagadish.