This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: TMS570LC4357 using CCS CCS_GNU_v9.3.1p1 linker flags -mfloat-abi=hard will causes link problem

Hi *

I have managed to compile target if change the linker setting to -mfloat-abi=soft, but this does not reflect this MCU TMS570LC43, which is cortex r5 and come -mfpu=vfpv3-d16. Based on the workaround suggest, I have already added the flags thru the miscellaneous as shown.

The compiler settings are based on the posts by the chester gillion (thanks a lot, appreciate your good support in the forum). Will like to seek help to overcome this issue.

Hope to hear from the rest too. Cheers.Deric