Part Number: TMDS243EVM
Other Parts Discussed in Thread: LP-AM243
Hello,
I got error message when I run QSPI example program.
Board: PROC101C
SDK: mcu_plus_sdk_am243x_08_05_00_24
Project: /ospi_flash_diag_am243x-evm
Error message shown in terminal:
----------------------------------------------------------------------------------------------------------
Starting NULL Bootloader ...
DMSC Firmware Version 8.5.3--v08.05.03 (Chill Capybar
DMSC Firmware revision 0x8
DMSC ABI revision 3.1
INFO: Bootloader_runCpu:155: CPU r5f1-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:155: CPU r5f1-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:155: CPU m4f0-0 is initialized to 400000000 Hz !!!
INFO: Bootloader_loadSelfCpu:207: CPU r5f0-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_loadSelfCpu:207: CPU r5f0-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runSelfCpu:217: All done, reseting self ...
[OSPI Flash Diagnostic Test] Starting ...
[OSPI Flash Diagnostic Test] Flash Manufacturer ID : 0xFF
[OSPI Flash Diagnostic Test] Flash Device ID : 0xFFFF
[OSPI Flash Diagnostic Test] Executing Flash Erase on first block...
[OSPI Flash Diagnostic Test] Erase Failed !!!
[OSPI Flash Diagnostic Test] Performing Write-Read Test...
[OSPI Flash Diagnostic Test] Wtite Failed !!!
ERROR: ospi_flash_diag_test_compare_buffers:181: OSPI read data mismatch !!!
Some tests have failed!!
----------------------------------------------------------------------------------------------------------------
Would someone please tell me where is the problem?
BR
JM