Part Number: SYSCONFIG
Other Parts Discussed in Thread: TMS320F280037
Sysconfig allows you to setup the reference for the ADC, however, you can only specify the voltage reference for the internal reference. The external reference can't be specified. In the device driver there are two options for an external voltage reference:
//*****************************************************************************
//
//! Values that can be passed to ADC_setVREF() and ADC_setOffsetTrimAll() as the
//! \e refVoltage parameter.
//!
//
//*****************************************************************************
typedef enum
{
ADC_REFERENCE_3_3V = 0U,
ADC_REFERENCE_2_5V = 1U
} ADC_ReferenceVoltage;
However, there is only one option possible in sysconfig:

If you switch to "Internal" reference, you get an option to specify the internal reference:

Is there a workaround so I don't have to edit the automatically generated files?
Regards