Part Number: MSPM0G3107
dear
Background: Power Policy is STANDBY0, TIMA0 is configured in PWM mode, DL events are published to event Channel 1, ADC subscribes to this channel as the sampling trigger source, stops Tima0(DL) and ADC (DL) after running for a few seconds, turn both off (disablePower) , force the PWM output down, and call WFI sleep.
At this time the current is 1.3 Ma, which is not expected, the power consumption is obviously too large. Based on the above background, with the TIMA0 publishing event cancelled (without calling the DL enable event or without calling the DL connect event channel) , the current during hibernation in Standby0 mode is 0.1 ma, which is expected.
Question: Why does a Tima0 release event cause sleep power to increase? It should not be expected. Information on the chip: 23AJ41WG4 XMOG Reva
thanks in advace